Kollmorgen Automation Suite RuntimeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running (commonly named the KAS Runtime) offers, in a single software package, the functionally of both a soft PLC"Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events and a motion controller.
The KAS Runtime (virtual machine) is a high-performance deterministic environment designed to run on different hardware platforms ranging from low-cost programmable drives to high-end Programmable Automation Controllers. This gives machine builders all the flexibility when designing their machines.
KASsupports many configurations when integrating machines:
The KAS Runtime can be used in the two different contexts:
See Different Implementations for more details.
|
Copyright © 2015 Kollmorgen™ |
|